AXIS#.HWEN.SOURCE
Description
Selects which digital input will be used as the hardware enable input for an axis. No hardware input is used if this is set to zero.
Examples
Usage
0: disables the hardware enable function
1 to 8: selects DIN# as the hardware enable input for an axis and is supported on all drive models.
9 to 12: selects DIN# as the hardware enable input for an axis on drives with X22 Extended I/O Connector
DIN3 is the default for axis 1
DIN4 is the default for axis 2
Code
-->AXIS1.HWEN.SOURCE 5
-->AXIS2.HWEN.SOURCE 5
Selects DIN5 as the hardware enable input for both axis 1 and axis 2.
-->AXIS1.HWEN.SOURCE 0
-->AXIS2.HWEN.SOURCE 6
Disables hardware enable function on axis 1 and selects DIN6 as the hardware enable input for axis 2.
Context
For more information on hardware enable, refer to the Enable/Disable.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 8, extended to 12 for drives with X22 Extended I/O Connector |
| Default Value | 3 for Axis 1, 4 for Axis 2 |
| Data Type | Integer |
| See Also | AXIS#.HWEN.STATE, AXIS#.HWEN.MODE |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HWEN.SOURCE | 0x5009 | 0x1 | USINT | - | - | RW | False |
| AXIS2.HWEN.SOURCE | 0x5109 | 0x1 | USINT | - | - | RW | False |